Arc Welding Assembly Dispensing & Sealing Inspection Laser Applications Laser Cutting Machine Tending Material Handling Material Removal Painting Palletizing Picking & Packaging Spot Welding Welding Welding Cobot

By Industry

All Industries
Aerospace Agriculture Alternative Energy Automotive Composites Construction Consumer Goods Die Cast, Foundry & Mold Electric Vehicles Electronics Fabricated Metals Food & Beverage Glass Job Shops Medical Device Oil & Gas Paper & Printing Pharmaceutical Plastics Warehousing White Goods Woodworking
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
FANUC Authorized System Integrators design, build, and support custom robotic systems with cross-industry expertise and local support backed by FANUC standards.
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
Work with a FANUC Authorized CNC integrator to build or upgrade your machining systems with expert local support and proven FANUC technology.
CNC Retrofit Providers
CNC Retrofit Providers
Modernize existing machine tools with the latest FANUC CNC controls. Extend machine life and boost productivity at a fraction of new equipment costs.
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
Solutions for Schools Solutions for Students Education Sales FANUC Academy Partners Scholarships Join the Automation Generation NOCTI Certifications Explore all Education →
Robotics Authorized System Integrators Ready to Go Solutions Automation Evaluation Authorized CNC System Integrators Retrofit Solutions Machining Evaluation Explore all How to Buy →
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
  3. Case Studies
  4. ›
  5. Rural Manufacturer Facing Welder Shortage Turns to FANUC’s Arc Welding Robots for Fabrication

Rural Manufacturer Facing Welder Shortage Turns to FANUC’s Arc Welding Robots for Fabrication

The Will-Burt Co. used FANUC welding robots to overcome labor shortages, improve weld quality, control costs, and increase capacity.

Solution By
Weldbot
Weldbot
Published
June 20, 2024
Last Updated September 11, 2026
Share Facebook X LinkedIn Email Copied link
Weldbot Video courtesy of Weldbot
A yellow overhead-mounted robotic arm performing a welding or cutting process on a metal automotive frame inside a black and yellow safety-fenced work cell.
QR code to view the full case study

Scan to watch the video

https://www.fanucamerica.com/case-studies/rural-manufacturer-facing-welder-shortage-turns-to-fanucs-arc-welding-robots-for-fabrication

Challenges

01

Skilled welder shortage causing staffing shortages.

02

Facing rising costs.

03

Manual welding of large parts could pose ergonomic and safety issues for employees.

Results

Proven technology 4

Efficiency keeps production costs low.

Product range 1

Gained production capacity and throughput via extended welding hours.

Young generation 3

Increasing employee safety.

Trending up 4

Higher quality parts produced with better welds.

A yellow overhead-mounted robotic arm performing a welding or cutting process on a metal automotive frame inside a black and yellow safety-fenced work cell.

Story

The Will-Burt Co. is an international OEM serving many different industries including defense, telecommunications, energy production and more. The campus in Orville, Ohio has over 250,000 square feet of manufacturing and assembly space. Part of the manufacturing activities done here is fabrication of sheet metal used by heavy machinery companies such as Caterpillar and JLG. Located in a rural area, the company was challenged with finding skilled welders and the welder shortage was affecting the company’s ability to take on additional work.

The company went from a manual welding process to an automated robotic arc welding system, integrated by Weldbot, using a FANUC M-710iC/12L robot for their large parts first in 2020 and added another automated system using a FANUC ARC Mate 100iD/8L robot. Will-Burt found that the robots were on average 3 to 4 times more efficient than manual welding, plus yielded better welding quality. For every robotic system added, it has allowed an extra 240 to 320 additional hours of welding per week or approximately $4 million of contract fabrication work. The extra capacity and capabilities allow the facility to control costs, keeping the company competitive while improving the quality of the parts produced.

Future automation projects include automating their CNC machine tending as well as adding another automated robotic welding solution.

Mike gibb quote image
"

I’ve been working with FANUC robots for over 20 years. They've just always proven to be extremely dependable. They've always been well supported on the technical side. And frankly, we've always just found them easy to interface with.

Mike Gibb Vice President of Operations – The Will-Burt Company

FANUC Products Used

Yellow FANUC M-710iC industrial robotic arm on a gray base, shown against a white background with its long arm extended upward and to the right.
Articulated Robots

M-710iC/12L

The FANUC M‑710iC/12L is a small to medium payload 6‑axis robot model ideal for all applications to handle medium payloads for up to 12 kg.

Max Payload:
12 kg
Reach:
3123 mm
View M-710iC/12L
FANUC ArcMate 100iD robotic welding arm in yellow, equipped with a Lincoln Electric AutoDrive wire feeder and MIG welding torch
Arc Welding

ARC Mate 100iD/8L

Long-arm arc welding robot ideally suited for working in compact robotic cells where extra reach is required for welding.

Max Payload:
8 kg
Reach:
2032 mm
View ARC Mate 100iD/8L
Weldbot
FANUC Authorized System Integrator

Weldbot

WeldBot is a FANUC exclusive integrator located in Akron, Ohio, focusing on the most challenging application in Robotics—Arc-Welding. With this focus, we are better able to meet the challenges associated with welding. Robotics and welding each require their own expertise, and when combined, a new and unique subset of skills are required to be successful. With being brand exclusive to FANUC, we truly understand the FANUC controller and can push the limits as needed.

Visit Website https://weldbot.com/
Cropped WB Vertical BW1
End User

Will-Burt Company

The Will-Burt Company is the world's premier manufacturer of mobile telescoping masts, towers, trailer systems, and pan and tilt positioners. We offer virtually every mobile payload elevation solution and full integration services for defense, government, first responders, telecommunications, energy production and other markets. Will-Burt also offers contract manufacturing, metal fabrication, powder-coating, and rapid prototyping services.

Visit Website