The start of a new year is a great time to evaluate the future of your production operations and discover what's possible with FANUC's reliable automation solutions.
FANUC America Booth #4500
Complete the form to be contacted by an automation expert > >
FANUC’s expanded series of CRX collaborative robots are extremely robust and able to run for eight years without maintenance. Easy-to-use interactive programming enables users to teach points using hand guidance or a Tablet TP with drag and drop icons.
A CRX-10iA with the Power Motion i-Model A (PMi-A) will simulate brake rotor assembly. The PMi-A moves parts into position for the CRX, presses a simulated rivet into the part, and performs quality inspection of the rivet press. FANUC's Robot ON-SITE enables the robot to control the functionality and actions through robotic programming with the ability to “talk” to the CNC G-code program.
A CRX-25iA robot, offering a 30kg payload and 1,889mm reach will demonstrate case palletizing. Guided by a 3DV/200 vision sensor mounted to the arm, the CRX-25iA will palletize boxes to nearly 7’ high. In addition, the CRX-25iA will be mounted to a mobile cart to showcase its flexibility. The robot can be easily repositioned by hand and uses vision to automatically adjust to its new location and continue working accurately.
A CRX-10iA demo showcases the cobot's ease of use. Customers can program the robot and experience it firsthand.
FANUC recently expanded its line of four-axis SCARA robots to include the SR-3iA/U ceiling mount featuring a full 360-degree work envelope with no dead zones, and the SR-3iA/C and SR-6iA/C cleanroom variants.
The SR-3iA/U ceiling mount SCARA robot has a 3kg payload and 350 mm reach. Featuring a full 360-degree work envelope with no dead zones, the robot can access any point within its reach. The SR-3iA/U will use iRVision 3DV and iRPickTool to pick various parts from a moving circular conveyor, move them to a 2D camera for inspection, then place them onto an outfeed conveyor into the appropriate Pass/Fail locations.
A FANUC SR-12iA robot with the Environmental Option will pack and unpack trays of medical vials into a bin, and then pick up and transfer a full bin to demonstrate the SR-12iA’s payload capability. The SR-12iA robot with the Environmental Option includes white epoxy coating, bellow covers, anti-rust bolts and seals, and an IP65 rating to withstand dust and liquids.
FANUC offers application software for packaging and palletizing, integrated iRVision® and tracking features, ROBOGUIDE simulation, Dual Check Safety (DCS), and Zero Down Time (ZDT) to help customers monitor and manage their automation.