888-FANUC-US
FABTECH 2021

FANUC Features Latest Robotic and Automation Solutions at FABTECH 2024

As a global leader in robotics and automation, we’re excited to showcase our latest innovations at FABTECH 2024, held at the Orange County Convention Center in Orlando, Florida - October 15-17.

What You’ll See:

Main Booth #W-4817: Welding and Laser Solutions

Discover our world-renowned welding and laser technologies. From precision welding to high-speed laser cutting, we’ve got you covered. Our experts will be on hand to demonstrate the reliability and efficiency of our solutions.

Paint Booth #W-2729: Introducing the CRX Paint Cobot

Meet the future of painting automation - our brand-new CRX Paint Cobot offering precision, flexibility, and ease of use. Whether it’s automotive coatings or intricate designs, the CRX Paint Cobot delivers flawless results.

Connect with Us:

Before the show, feel free to reach out. Our welding and fabrication experts are here to answer your questions and discuss your unique needs. Fill out the form, and we’ll be in touch right away.

 
 
 
 
CRX Product Lineup

Collaborative Robots

FANUC’s diverse range of CRX cobots will be on display, featuring a variety of materials joining applications while showcasing cost-effective solutions that can handle low or high-volume part runs, for any size part, at any reach or payload to fit your needs.

Demonstrating the flexibility of cobots for welding near human operators, a CRX-10iA/L cobot—mounted on a 7th axis rail—will simulate welding at one station while an operator loads the second station.

See Our Solutions at FABTECH Orlando
Main Booth #W4817 and our Paint Pavilion Booth #W2729


As the global leader in automation and robotics, we’re committed to providing solutions that help our customers achieve their production goals and overcome labor challenges. See a sampling of other products we’ll demonstrate at FABTECH.

Heavy lifting and material handling robots for even the toughest tasks

M-950 Fiction Stir Weld Demo

Friction Stir Welding with M-950iA/500 Robot

New to the FANUC Lineup, the M-950iA/500 heavyweight robot features a wider range of motion, offering an impressive 500 kg payload capacity and 2,830 mm reach, showcased in a new friction stir welding demonstration featuring a StirRob Friction Stir Welding Head by FPT Industrie.

M-800 Ultra Accurate High Speed Precision Laser Cutting Demo

M-800/60-20B High Speed Laser Cutting

The new M-800/60-20B, FANUC’s next-gen, high-accuracy industrial robot, makes its FABTECH debut. Shown with FANUC’s high-speed laser interface connected to a TRUMPF TRUFiber 4001 P and LaserMech FiberCUT STa to showcase high-speed laser cutting. Cut holes are generated with Shape Gen software for easy single point teaching.

 CRX-10iA Welding Demo

Welding with CRX-10iA/L

The ideal solution for manufacturers with little to no robotic experience, the CRX-10iA/L cobot—with a 10 kg payload and 1,418 mm reach—offers an all-new FANUC programming interface with buttons on the wrist to create welding programs, and integrated aux-axis to properly position parts for welding. The ease of programming paired with FANUC’s world-renowned technology, proven reliability and sensitive contact detection demonstrates the flexibility of cobots for welding in many applications.

Flexible Multi-Arm Welding with R-1000iA/100F

A FANUC R-1000iA/100F material handling robot uses iRVision® 3DV to locate and pick an auger from a rack and present it to an ARC Mate 100iD welding robot. Showcasing the flexibility of coordinated motion, the ARC Mate simulates welding the auger ‘flight to shaft’ as the R-1000iA rotates the part. Next, the R-1000iA repositions the augur and the ARC Mate uses SERVO ROBOT’s FUJI-CAM 2.0 sensor to track the augur’s outer edge and simulates hard face welding as the R-1000iA rotates the part to maintain a flat welding position.

FANUC Paint Robot Line-Up 

Paint Robots and Cobots

FANUC’s new CRX-10iA/L Paint cobot, the first explosion-proof collaborative paint robot available globally, will be prominently featured at FANUC’s Paint Pavilion Booth. Demonstrations will show how easy the cobot is to setup and use, even for companies with little to no robotic experience.

In addition, FANUC’s P-40iA will be showcased utilizing Visual Tracking for PaintTOOL software, which is designed to help boost customers’ paint quality. This robot will work alongside a CRX-20iA using iRPickTOOL and iRVision software to load/unload guitars to be “painted” by the P-40iA.

ALPHA i-D Series Servo Motor

Factory Automation

For CNC-focused demonstrations, FANUC America will be featuring a display of products we offer machine tool builders to go to market with the best equipment possible, including our new Alpha i-D Servo System as well as CNCs for laser cutting machines. Plus, we’ll have a CRX machine load and unload a lathe using FANUC’s Robot G-code feature, which allows a FANUC robot to be controlled via G-code through the FANUC CNC.

LETS TALK AUTOMATION

FANUC's solutions help companies maximize profits, overcome labor issues and stay competitive. Ready to automate? Let's Talk!

888-FANUC-US