Skip to content Skip to navigation
Resources About MyPortal Login
Edit Entry
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
Arc Welding Assembly Dispensing & Sealing Inspection Laser Applications Laser Cutting Machine Tending Material Handling Material Removal Painting Palletizing Picking & Packaging Spot Welding Welding Welding Cobot

By Industry

All Industries
Aerospace Agriculture Alternative Energy Automotive Composites Construction Consumer Goods Die Cast, Foundry & Mold Electric Vehicles Electronics Fabricated Metals Food & Beverage Glass Job Shops Medical Device Oil & Gas Paper & Printing Pharmaceutical Plastics Warehousing White Goods Woodworking
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
FANUC Authorized System Integrators design, build, and support custom robotic systems with cross-industry expertise and local support backed by FANUC standards.
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
Work with a FANUC Authorized CNC integrator to build or upgrade your machining systems with expert local support and proven FANUC technology.
CNC Retrofit Providers
CNC Retrofit Providers
Modernize existing machine tools with the latest FANUC CNC controls. Extend machine life and boost productivity at a fraction of new equipment costs.
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
Solutions for Schools Solutions for Students Education Sales FANUC Academy Partners Scholarships Join the Automation Generation NOCTI Certifications Explore all Education →
Robotics Authorized System Integrators Ready to Go Solutions Automation Evaluation Authorized CNC System Integrators Retrofit Solutions Machining Evaluation Explore all How to Buy →
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
  3. Case Studies
  4. ›
  5. Swivellink Boosts Output 33% with Robotic ROBODRILL Tending

Swivellink Boosts Output 33% with Robotic ROBODRILL Tending

Swivellink overcame labor shortages, boosted output by 33%, and delivered fast ROI by automating ROBODRILL machine tending with FANUC robots.

Solution By
APT
APT
Published
June 5, 2023
Last Updated August 25, 2026
Share Facebook X LinkedIn Email Copied link
APT Video courtesy of APT
Swivellink Thumbnail
QR code to view the full case study

Scan to watch the video

https://www.fanucamerica.com/case-studies/robotic-cnc-machine-tending-automation-increases-production-and-roi

Challenges

01

Needed to increase part production in a limited space.

02

Experiencing a labor shortage.

03

The part needed to be deburred on its many edges, including on the underside.

Results

Proven technology 8

1.5 minutes saved per part

Product range 4

$1.74 saved per part:

Quality improvement 3

1500 parts per week (2 shifts, 5 days)

Maintenance health 2

$2610 saved per week

Optimization 8

33 weeks ROI

Swivellink Thumbnail

Story

Swivellink manufacturers mounting systems used for vision systems, cycle start buttons, sensors, light monitors and robotic applications in Northwest Ohio. Parts are machined on two ROBODRILLS for 20-24 hours a day. However, the company was facing a shortage of labor to operate the machines and needed to boost production to keep up with demand.

APT Manufacturing Solutions, a FANUC-certified robotics integrator, implemented an automated machine tending solution using LR Mates with the ROBODRILLS to load and unload parts. The automation has resulted in a 33% increase in production efficiency and an ROI of just 33 weeks. The CNC cycle time did actually increase by 20 seconds with the FANUC robot, but the total cycle time actually decreased by 1:30 over an 8-hour shift because of the robot’s excellent accuracy and reliability. The number of parts produced over the 8-hour shift increased from 100 to over 150 with the robotics application.

Roger Sanders
"

We're able to get more product out with the same amount of labor.

Roger Sanders Product Developer – Swivellink

FANUC Products Used

LR Mate 200iD
Articulated Robots

LR Mate 200iD

The FANUC LR Mate 200iD is a compact 6 axis robot with best-in-class robot weight-load capacity, IP67 protection, and outstanding FANUC quality.

Max Payload:
7 kg
Reach:
717 mm
View LR Mate 200iD
M 10id 16s Beauty Shot
Articulated Robots

M-10iD/16S

The FANUC M‑10iD/16S is a compact short-arm 6‑axis robot designed for tight workspaces, offering high versatility and support for top-mount applications.

Max Payload:
16 kg
Reach:
1103 mm
View M-10iD/16S
APT
FANUC Authorized System Integrator

APT

APT Manufacturing Solutions has been providing high-tech solutions to manufacturing problems for our customers since 1996. Founded initially in a 2500 square foot facility as machining and machine building, APT is now manufacturing in a 100,000 square foot facility with state-of-the art equipment, technology, and people. Our operations are ISO 9001 certified. We are an authorized FANUC robotic integrator and certified at the highest level (V), as well as being an A3 Certified Robot Integrator.

Visit Website https://www.aptmfg.com
Swivellink
End User

Swivellink

Swivellink manufacturers mounting systems used for vision systems, cycle start buttons, sensors, light monitors and robotic applications in Northwest Ohio.

Visit Website