CNC Strategic Communications Specialist
The FANUC Tablet Teach Pendant Plug-in SDK allows you to create unique
graphical icons and screens.
Cobots are flexible for all types of applications, and with FANUC’s
Tablet Teach Pendant (TP) Plug-in SDK, so are the User Interfaces. Plug-in
SDK, short for Software Developer’s Kit, is an HTML5/JavaScript-based
platform enabling the creation of specific icons for the Tablet TP’s
timeline editor as well as to make dedicated screens on the HMI. This allows you to create a streamlined, efficient, custom HMI to ensure that cobot operation is as simple and straightforward as you need it to be.
The personalized screens of the custom HMI are full-sized pages, which allow the setup of
peripheral devices or interactions with the work cell on the Cobot’s
Tablet TP. Additionally, custom icons can be created to perform tasks
specific to your application. FANUC created dedicated screens and icons in our
collaborative robot bicycle assembly demonstration.
The Cobot Bicycle Assembly Use Case
In FANUC’s CR-35iB
collaborative robot bicycle assembly demonstration, we created icons on the custom HMI that prompt the user to assemble and inspect the bicycle at certain points in
the program after the robot had oriented the bicycle for convenient access
for the user.
Additionally, a custom work cell HMI can be created using Plug-in SDK, as we
also did in the bicycle assembly demonstration. In the video, you can see
where the user checks each step along the assembly process. When finishing one
step, a “confirm” button is pressed on the custom HMI, and the robot moves to the
next assembly position, where a new set of instructions is displayed. These
elements on the Tablet TP were all created via Plug-in SDK.
Custom icons can also be created, which are geared towards your application
and can output a custom error. These icons on the Cobot’s Tablet TP can
be programmed to complete whatever action you need.
Start Programming Your Custom HMI
To make programming with the Tablet TP SDK easier, FANUC provides
preloaded iHMI Components for all controllers with the Tablet TP option. These are
uniform FANUC stylesheets for controls, such as buttons and drop-down
selection boxes.
You are not limited to these styles, however. In addition to these iHMI components, you are able to use any standard HTML that you might be
familiar with or already using.
For the creation of webpages, we offer JavaScript built-ins for handling the
communication between your screen and the controller. This would be used for
setting or reading values or variables.
Plug-in SDK for Tablet TP Your Way
The SDK allows the generation of structured-text code to fully customize the
Tablet TP. Those comfortable with JavaScript programming may create custom
icons for use in the timeline editor for programming macros and may design
fully intuitive HMI screens suitable to specific needs. This allows you to
utilize your FANUC Tablet TP as the primary HMI interface for simple cells
rather than needing to purchase 3rd party equipment.
The Tablet TP Plug-in SDK extends the functionality of FANUC’s robot
programming language, making FANUC Cobots even more flexible and tailor-made
for your needs.