See FANUC at Amazon’s re:MARS Tech Showcase where we’ll demonstrate how easy it is to program and use a FANUC cobot.
ROCHESTER HILLS, MI – (May 30, 2019) – FANUC America, the leading supplier of robotics, CNCs and ROBOMACHINEs has expanded its line of easy to use collaborative robots to include six models. Look for FANUC at Amazon’s re:MARS Tech Showcase (June 4-7 in Las Vegas) where we’ll demonstrate how easy it is to program and use a FANUC CR-7iA collaborative robot.
FANUC’s series of power and force limiting collaborative robots can handle 4-35 kg payloads and a 550-1813 mm reach. Easy to program and use – even for those with little or no experience - FANUC’s cobots are equipped with FANUC’s iHMI intuitive touch screen user interface that includes step-by-step programming instructions right from the teach pendant. Simple and straightforward programming helps reduce costs associated with operator training, minimizes setup time and increases system productivity. In addition, FANUC’s Hand Guidance feature allows operators to teach a collaborative robot by leading it through paths at the press of a button and/or use it to lift heavy objects manually.
FANUC’s six cobot models combine world-renowned automation technology, proven reliability and very sensitive built-in sensors that allow them to work safely alongside people in a variety of industrial/manufacturing jobs including machine tending, dispensing, inspection, kitting, palletizing, e-commerce, and more. In addition, FANUC’s collaborative robots are equipped with intelligent options such as iRVision® and force sensing.
“We offer the industry’s widest range of collaborative robots in terms of payload, reach and speed options,” said Amanda Nixon, collaborative robot product manager, FANUC America. “In addition, our cobots are very easy to program with FANUC’s Hand Guidance or the iHMI touch screen, and provide easy plug-and-play for intelligent options like vision and force sensing. No other cobot brand in the world can offer what FANUC provides to our customers, including lifetime product support.”
Learn more about FANUC’s line of easy to use collaborative robots at: https://www.fanucamerica.com/cobots.
About FANUC America Corporation
FANUC America Corporation is a subsidiary of FANUC CORPORATION in Japan, and provides industry-leading robotics, CNC systems, and factory automation. FANUC’s innovative technologies and proven expertise help manufacturers in the Americas maximize productivity, reliability and profitability.
FANUC embraces a culture of “Service First” which means that customer service is our highest priority. We are committed to supplying our customers with parts and support for the life of their FANUC products.
FANUC America is headquartered at 3900 W. Hamlin Road, Rochester Hills, MI 48309, and has facilities in: Atlanta; Boston; Charlotte; Chicago; Cincinnati; Cleveland; Houston; Los Angeles; Minneapolis; Montreal; Pine Brook, NJ; Pontiac, MI; San Francisco; Seattle; Toronto; Buenos Aires, Argentina; Sao Paulo, and Manaus, Brazil; and Aguascalientes, Monterrey, and Queretaro, Mexico. For more information, please call: 888-FANUC-US (888-326-8287) or visit our website: www.fanucamerica.com. Also, connect with us on YouTube, Twitter, Facebook, LinkedIn and Instagram.
FANUC America Corporation PR contacts:
Cathy Powell
Public Relations and Communications Manager
FANUC America Corporation
T: 248-377-7570
E: [email protected]
Derek Sheedy
Marketing Communications Specialist - CNC
FANUC America Corporation
T: 847-898-5679
E: [email protected]
###