Interested in a FANUC Product or Solution?

Contact us to receive more information on any product/solution, or to request a price quote. We'll be happy to answer any questions you may have, simply click below to get started.

Contact Us

FANUC America Press Releases

The latest news and product updates from the world's leading supplier of factory automation. For media inquiries, please email Public Relations.


FANUC CNC and Robotics Integration Simplifies Operations

The new feature enables FANUC CNCs to directly program robots through the G-code.
by FANUC America | Mar 16, 2021

FANUC CNC and Robotics Integration Simplifies Operations

The new feature enables FANUC CNCs to directly program robots through the G-code.     

HOFFMAN ESTATES, IL – FANUC America, a leading factory automation solutions provider, introduces the next step in complete robotics and CNCs integration for more efficient operations. FANUC CNCs now have the ability to control connected FANUC robots providing machine tending or other assistance through FANUC’s Robot and CNC Integration.

More manufacturing operations are taking advantage of adding more robotics to execute repetitive tasks previously manually performed. Advanced automation offers a competitive edge and greater profit margins to shops of all sizes.

FANUC’s Robot and CNC Integration is a complete package that simplifies the connection of a FANUC robot to a FANUC controlled machine tool. The new Robot G-code feature allows operators and machine tool builders to program robots easily through the FANUC CNC in ISO standard G-code format. Those unfamiliar with robotic programming language will no longer require additional training or specialists because the programming can be performed with G-codes. A reliance on a separate teach pendant for the robot is also greatly reduced with the capability of robotic programming and operation through the CNC user interface. 

FANUC’s Robot and CNC Integration not only makes connecting a FANUC robot through a high-speed Ethernet cable to a machine tool easy, but also simplifies the setup, programming and operation. The Robot G-code feature is available on FANUC CNC Series 0i-F, 0i-F Plus, 30i-B and 30i-B Plus.

 

About FANUC America Corporation

FANUC America Corporation is a subsidiary of FANUC CORPORATION in Japan, and provides industry-leading robotics, CNC systems, and factory automation.  FANUC’s innovative technologies and proven expertise help manufacturers in the Americas maximize productivity, reliability and profitability. 

FANUC embraces a culture of “Service First” which means that customer service is our highest priority.  We are committed to supplying our customers with parts and support for the life of their FANUC products.   

FANUC America is headquartered at 3900 W. Hamlin Road, Rochester Hills, MI 48309, and has facilities in:  Auburn Hills, MI; Atlanta; Boston; Charlotte; Chicago; Cincinnati; Houston; Huntington Beach, CA; Los Angeles; Minneapolis; Montreal; Pine Brook, NJ; Pontiac, MI; Birmingham, AL; San Francisco; Seattle; Toronto; Buenos Aires, Argentina; Sao Paulo, and Manaus, Brazil; and Aguascalientes, Monterrey, and Queretaro, Mexico.  For more information, please call: 888-FANUC-US (888-326-8287) or visit our website: www.fanucamerica.com .  Also, connect with us on YouTube, Twitter, Facebook, LinkedIn and Instagram

 

FANUC America Corporation PR contact:

Factory Automation: Debra Schug
CNC Strategic Communications Specialist
T: 847.898.5673
E: [email protected]

Robotics: Cathy Powell
Public Relations and Communications Manager
FANUC America Corporation
T: 248-377-7570
E: [email protected]

###