Interested in a FANUC Product or Solution?

Contact us to receive more information on any product/solution, or to request a price quote. We'll be happy to answer any questions you may have, simply click below to get started.

Contact Us

FANUC America Press Releases

The latest news and product updates from the world's leading supplier of factory automation. For media inquiries, please email Public Relations.


FANUC Showcases CRX Cobots at The Battery Show North America

FANUC will demonstrate its popular line of CRX collaborative robots at The Battery Show North America in Novi, Mich., Sept. 13-15, booth #2626.
by FANUC America | Aug 26, 2022

ROCHESTER HILLS, MI – (Aug. 26, 2022) – FANUC, the global leader in CNCs, robotics and ROBOMACHINEs will demonstrate its popular line of CRX collaborative robots at The Battery Show North America in Novi, Mich., Sept. 13-15, booth #2626.    

FANUC’s CRX cobots are extremely robust and able to run for up to eight years without maintenance.  Interactive programming enables users to teach points using hand guidance or a tablet interface with drag and drop icons.  Following the success of the CRX-10iA and CRX-10iA/L, three new models were introduced this year including the CRX-5iA, CRX-20iA/L and CRX-25iA.   The expanding cobot series can handle products from 5kg to 25kg and reach capabilities from 994mm to 1,889mm.   

There are now 11 FANUC CR and CRX cobot models available to help the battery, EV and other industries with production applications such as inspection, machine load/unload, packing, palletizing, sanding, welding, and many more.     

At the show, a FANUC CRX-10iA will provide attendees the opportunity to try the cobot’s intuitive hand guidance and easy-to-use tablet programming.  

In a second demonstration, a CRX-10iA/L will use AI Error Proofing to inspect for the presence/absence of components on steering wheels.  FANUC’s AI Error Proofing is a function in iRVision® designed for part inspection that uses machine-learning technology.  The CRX-10iA/L equipped with a robot-mounted camera will inspect two steering wheels to determine passed or failed samples.  The steering wheels will be fixed to a table but can be rotated by an operator to show that the robot is able to inspect non-fixtured parts. 

Click here for more information about FANUC’s automated solutions for EV processes.   

About FANUC America Corporation

FANUC America Corporation is a subsidiary of FANUC CORPORATION in Japan, and provides industry-leading CNC systems, robotics and factory automation.  FANUC’s innovative technologies and proven expertise help companies in the Americas maximize productivity, reliability and profitability. 

FANUC America is headquartered at 3900 W. Hamlin Road, Rochester Hills, MI 48309, and has facilities throughout North and South America.  For more information, please call: 888-FANUC-US (888-326-8287) or visit our website: www.fanucamerica.com .  Also, connect with us on YouTube, Twitter, Facebook, LinkedIn and Instagram

FANUC America Corporation PR contact:

Robotics: Cathy Powell
Public Relations and Communications Manager
FANUC America Corporation
T: 248-377-7570
E: [email protected]

Factory Automation: Debra Schug
CNC Strategic Communications Specialist
T: 847.898.5673
E: [email protected]

                                                                    ###