FANUC America will showcase a wide range of automation technologies including new CRX Cobot welders at FABTECH in Atlanta, Nov. 8-10. See FANUC at its main booth #C11637 and at the Painting Pavilion in booth #B5335.
ROCHESTER HILLS, MI – (Nov. 6, 2022) – FANUC,
the global leader in CNCs, robotics and ROBOMACHINEs will showcase a wide
range of automation technologies including new CRX Cobot welders at FABTECH
in Atlanta, Nov. 8-10. See FANUC at its main booth #C11637 and at the
Painting Pavilion in booth #B5335.
New CRX Welders
FANUC’s new CRX 25iA cobot is extremely robust and able to run
for up to eight years without maintenance. At FABTECH, FANUC will
showcase the new CRX-25iA welding cobot, which offers a 25kg
payload and 1,889mm reach. In addition, a CRX-10iA welding
cobot will allow attendees to teach weld joints using hand guidance or a
tablet interface with drag and drop icons. The easy-to-use CRX welding
cobots support FANUC’s advanced features including iRVision®, Torch Angle Control,
Touch Sensing and Thru Arc Seam Tracking (TAST).
In 2022, FANUC expanded its popular series of CRX
collaborative robots with the new CRX-5iA,
CRX-20iA/L and CRX-25iA. Now with a total of 11 CR
and CRX cobot model variations, FANUC has a cobot to handle products ranging
from 4 to 35kg in applications such as welding, inspection, machine
load/unload, packing, palletizing, sanding, and more.
Heavy Part Welding with ARC Mate 100iD Robot
A FANUC ARC Mate 100iD robot picks a part from a part feeder and
loads it into a t-joint fixture. The ARC Mate 100iD uses
FANUC’s Seam Tracking software with SERVO ROBOT’s FUJI-CAM 2.0
sensor to track and weld the first pass with Lincoln Electric’s
Hyperfill®. A one-axis positioner repositions parts for
welding the left and right sides of the t-joint. Light shields lower
to show attendees completed parts and the cycle repeats. The
demonstration also features the Lincoln Electric Power Wave® R450
robotic power source with the Advanced Module using the GMAW Pulse
process.
This efficient robotic welding solution is easy to setup and provides maximum
weld deposition with improved cycle times.
The ARC Mate 100iD robot is the latest member of FANUC’s ARC Mate series based on the experience gained
in providing arc welding robots for 40 years. Designed specifically
for arc welding, laser welding, soldering, and cutting applications, the ARC
Mate robots are rated best-in-class for speed and accuracy.
A sleek and lightweight design features internal cable routing and a curved
J2 robot arm, minimizing interference with work pieces and fixtures and
allowing more productivity in the work area. The series, which
includes the larger ARC Mate 120iD, also features a long reach and
stroke - even in the backflip region – making it easier for customers
to apply the robot while maximizing their available workspace –
including larger parts or tooling.
Robotic Trimming and Spot Welding
The R-2000iC/190S and R-2000iD/210FH are members
of an extensive family of industrial robots offering a variety of payloads
and reaches. A compact design and hollow arm provides better cable
management, minimizes interference with system equipment and makes it easier
to operate in tight workspaces. The R-2000iD/210FH has a
210kg payload and 2,605mm reach, and the R-2000iC/190S offers a 190kg
payload and 2,040mm reach. The popular R-2000 series is ideal for spot
welding, and a wide range of material handling and removal applications.
At the show, the R-2000iD/210FH robot equipped with integrated FANUC
Servo Gun Control and a hollow arm for spot welding dress out will perform
simulated spot welding in and around a truck cab. In addition, the
R-2000iC/190S robot will demonstrate trimming an airline
fuselage.
New Factory Automation
Industrial PCs for All Needs: FANUC offers industrial PCs providing a
powerful platform for custom developments in a wide variety of
applications. Available in several different sizes and options,
FANUC’s industrial PCs are fast, secure and easy to
use.
CNC Laser Solutions: FANUC’s new CNC laser solutions provide a seamless
connection to laser machines. FANUC’s dedicated CNCs for lasers
are highly synchronized with axis control to achieve high-precision
processing with various laser sources.
Retrofit Solutions: FANUC’s new CNC Retrofit Kits upgrade machine tools to
improve the performance of legacy machines. For those interested in
getting started, download the CNC Retrofit App to help collect and submit
relevant machine information.
Robotic Painting
A FANUC P-40iA paint robot equipped with the
R-30iB Plus Mate controller will demonstrate painting metal
furniture parts using integrated PaintPRO for cad-to-path programming to
achieve easy offline teaching and file transfer to the robot.
The system uses FANUC aux axis control with a table controlled by
FANUC’s Purge Motor Box solution. This feature enables part painting
with coordinated motion between the robot and the table’s
rotation.
The P-40iA robot has a 1,300 mm reach and a 5 kg payload, while
offering a compact arm design that fits into small work areas. It includes a
cast aluminum body, purged and pressurized arm, FANUC’s purge module,
and integrated solenoid valves for gun trigger. Whether the application
calls for liquid, powder, FRP chop or gel, the FANUC P-40iA is
ready for any applicator and application equipment, making it a complete
solution for painting.
Additionally, the P-40iA robot can be mounted in a variety of
positions including floor, invert, wall or angle mounts, benefitting
companies that are challenged with small or narrow workspaces. In
addition, the P-40iA can be programmed offline using FANUC
PaintTool Robot Software, and utilizes FANUC’s latest high-performance
R-30iB Mate Plus robot controller.
Since 1982, FANUC has designed and built its paint robots in the U.S. at
FANUC America’s headquarters in Rochester Hills, Michigan. Learn more about the P-40iA.
About FANUC America Corporation
FANUC America Corporation is a subsidiary of FANUC CORPORATION in Japan, and
provides industry-leading CNC systems, robotics and factory
automation. FANUC’s innovative technologies and proven expertise
help manufacturers in the Americas maximize productivity, reliability and
profitability.
FANUC America is headquartered at 3900 W. Hamlin Road, Rochester Hills, MI
48309, and has facilities throughout North and South America. For more
information, please call: 888-FANUC-US (888-326-8287) or visit our website:
www.fanucamerica.com . Also, connect with us on YouTube, Twitter, Facebook,
LinkedIn and Instagram.
FANUC America Corporation PR contact:
Robotics: Cathy Powell
Public Relations and Communications
Manager
FANUC America Corporation
T: 248-377-7570
E: cathy.powell@fanucamerica.com
Factory Automation: Debra Schug
CNC Strategic Communications
Specialist
T: 847.898.5673
E: debra.schug@fanucamerica.com
###