Interested in a FANUC Product or Solution?

Contact us to receive more information on any product/solution, or to request a price quote. We'll be happy to answer any questions you may have, simply click below to get started.

Contact Us

FANUC America Press Releases

The latest news and product updates from the world's leading supplier of factory automation. For media inquiries, please email Public Relations.


FANUC to Demonstrate CNC and Robotic Solutions for the Woodworking Industry at AWFS Fair

FANUC America is excited to return to tradeshows and we look forward to seeing you at the 2021 AWFS Fair.
by FANUC America | Jun 23, 2023

ROCHESTER HILLS, MI – (June 23, 2021) – FANUC America, the leading supplier of CNCs, robotics, and ROBOMACHINEs will demonstrate automated solutions for the construction, furniture, cabinet, and other woodworking industries at the AWFS Fair, July 20-23 in Las Vegas in booth #3075. 

Factory Automation Demonstrations

FANUC’s Factory Automation division is introducing an exciting way to see part production. Our Visual Twin demonstration highlights FANUC’s end-to-end digitalization solutions for the machine shop. By seamlessly working with various machine tool builders as well as Mastercam and ModuleWorks, FANUC’s Visual Twin is an exact software replica of real CNC machine tools. The Visual Twin will display a virtualized 5-axis machine tool cutting a part, which mirrors the real-world machine’s behavior.

Also from the Factory Automation division, we are demonstrating the seamless integration and high performance of FANUC’s CNC and servo systems in a Laguna iQ desktop CNC router. Equipped with a complete FANUC CNC system, the display shows how well the machine, control and drives all work together to bring unbeatable value in reliability and accuracy.

CRX Collaborative Robot Demonstration 

FANUC’s CRX cobot is an easy-to-use and versatile solution for a variety of applications, including sanding wood products like furniture, musical instruments, cabinets, containers and more.   A FANUC CRX cobot will demonstrate sanding wood guitars.   Visitors are welcome to try the easy hand guidance and tablet programming features. 

FANUC’s CRX collaborative robot offers the same high level of performance that all FANUC products are known for including the latest technologies and world-renowned reliability.  Built-in sensors on each axis allows the CRX cobot to work safely alongside people without the need for expensive guarding. 

In addition, interactive programming allows users to teach points using hand guidance or a new tablet interface with drag and drop icons.  The CRX cobot supports several of FANUC’s advanced features including iRVision,  and is a perfect fit for any application where collaborative robots can help customers achieve higher efficiencies.  Click here to watch the FANUC CRX in a wide range of applications. 

Technology & Innovation Session

Attendees should not miss the chance to hear Jim Cooper, general manager at FANUC America present “How to Evaluate Woodworking Robotic Applications” on Tuesday, July 20 at 11:30 a.m.   Jim’s discussion will cover advancements in robotic technologies that have made it easier for both small and large woodworking shops to implement automation.  Topics will include how to identify a good application, and recommendations on next steps, including how to determine if a collaborative robot may be a good fit.   

About FANUC America Corporation

FANUC America Corporation is a subsidiary of FANUC CORPORATION in Japan, and provides industry-leading CNC systems, robotics and factory automation.  FANUC’s innovative technologies and proven expertise help manufacturers in the Americas maximize productivity, reliability and profitability. 

FANUC embraces a culture of “Service First” which means that customer service is our highest priority.  We are committed to supplying our customers with parts and support for the life of their FANUC products.   

FANUC America is headquartered at 3900 W. Hamlin Road, Rochester Hills, MI 48309, and has facilities in:  Auburn Hills, MI; Atlanta; Boston; Charlotte; Chicago; Cincinnati; Cleveland; Houston; Huntington Beach, CA; Los Angeles; Minneapolis; Montreal; Pine Brook, NJ; Pontiac, MI; Birmingham, AL; San Francisco; Seattle; Toronto; Buenos Aires, Argentina; Sao Paulo, and Manaus, Brazil; and Aguascalientes, Monterrey, and Queretaro, Mexico.  For more information, please call: 888-FANUC-US (888-326-8287) or visit our website: www.fanucamerica.com .  Also, connect with us on YouTube, Twitter, Facebook, LinkedIn and Instagram

 

FANUC America Corporation PR contact:

Robotics: Cathy Powell
Public Relations and Communications Manager
FANUC America Corporation
T: 248-377-7570
E: [email protected]

 

Factory Automation: Debra Schug
CNC Strategic Communications Specialist
T: 847.898.5673
E: [email protected]
                                                             ###