FANUC America, a world leader in CNCs, robotics, and ROBOMACHINEs will demonstrate its latest robotic solutions for the battery and EV industries at the Battery Show, Sept. 12-14 in Novi, Mich., Booth #2545.
For Immediate Release
ROCHESTER HILLS, MI – (Sept. 5, 2023) – FANUC
America, a world leader in CNCs, robotics, and ROBOMACHINEs will demonstrate
its latest robotic solutions for the battery and EV industries at the Battery Show, Sept. 12-14 in
Novi, Mich., Booth
#2545.
FANUC CRX Cobots Demonstrate Enhanced Payload Capacity and AI Inspection
FANUC has expanded the payload capacities of its CRX and CR cobot lines to
handle products from 4 to 50kg. FANUC now has 11 cobot model variations that
can work in a variety of industrial applications including assembly,
inspection, material handling, packaging, palletizing, sanding, welding, and
more.
At the show, the CRX-25iA cobot will
demonstrate its
enhanced 30kg payload capacity by easily handling a 30kg kettlebell with
full wrist articulation.
In addition, a FANUC CRX-10iA cobot equipped with AI iRVision®
inspects batteries. Battery cells are placed on a table for AI vision
inspection by the cobot. The AI vision system compares example images to
actual parts as a reference. The compiled image data creates a strong basis
for comparison resulting in accurate inspection without requiring a
time-consuming setup. The accuracy of AI vision inspection results in better
quality control and part consistency.
FANUC’s entire series of CRX collaborative robots are
reliable,
flexible, and can work for eight years without maintenance. Easy-to-use
interactive programming allows operators to teach points using hand guidance
or a Tablet TP with drag and drop icons.
FANUC SR-20iA SCARA Robot Handling Batteries
At the show, FANUC’s SR-20iA SCARA robot demonstrates moving
car batteries between two trays. The demonstration shows the SR-20iA’s
ability to precisely handle heavy parts in a wide operating area at high
speeds.
The SR-20iA SCARA robot provides flexibility with a large vertical
stroke and offers an environmental option for harsh conditions.
All of FANUC’s SCARA robots use
iRProgrammer
– a web-based interface that lets you program the robot easily and
intuitively with a tablet or desktop computer or by using an optional Teach
Pendant.
About FANUC America Corporation
FANUC America Corporation is a subsidiary of FANUC CORPORATION in Japan, and
provides industry-leading CNC systems, robotics and ROBOMACHINEs.
FANUC’s innovative technologies and proven expertise help
manufacturers in the Americas maximize productivity, reliability and
profitability.
FANUC America is headquartered at 3900 W. Hamlin Road, Rochester Hills, MI
48309, and has facilities throughout North and South America. For more
information, please call: 888-FANUC-US (888-326-8287) or visit our website:
www.fanucamerica.com
. Also, connect with us on YouTube, Twitter,
Facebook,
LinkedIn and Instagram.
FANUC America Corporation PR contact:
Robotics: Cathy Powell
Public Relations and
Communications Manager
FANUC America Corporation
T: 248-377-7570
E:
[email protected]
Factory Automation: Debra Schug
CNC Strategic
Communications Specialist
T: 847.898.5673
E: [email protected]