Interested in a FANUC Product or Solution?

Contact us to receive more information on any product/solution, or to request a price quote. We'll be happy to answer any questions you may have, simply click below to get started.

Contact Us

FANUC America Press Releases

The latest news and product updates from the world's leading supplier of factory automation. For media inquiries, please email Public Relations.


FANUC Canada Demonstrates Latest Automation Solutions at CMTS

FANUC Canada, a leading supplier of CNCs, robotics, and ROBOMACHINEs will demonstrate its latest robotic and automation solutions at CMTS, Sept. 25-28 in Toronto, Ont., Booth #1429.
by FANUC America | Sep 08, 2023

 

For Immediate Release

MISSISSAUGA, ONTARIO – (Sept. 8, 2023) – FANUC Canada, a leading supplier of CNCs, robotics, and ROBOMACHINEs will demonstrate its latest robotic and automation solutions at CMTS, Sept. 25-28 in Toronto, Ont., Booth #1429.

FANUC CRX-10iA Assembly with the Power Motion i-Model A

A CRX-10iA with the Power Motion i-Model A (PMi-A) will simulate brake rotor assembly. The PMi-A moves parts into position for the CRX, presses a simulated rivet into the part, and performs quality inspection of the rivet press. The demonstration shows the versatility of the CRX cobot combined with the PMi-A, a high-performance and scalable general motion control supporting applications that require one to 32 axes.

The PMi-A, which offers CNC-style motion control for automated assembly and other applications, integrates seamlessly into virtually any production system using ethernet connection for easy communication between robots and machines. Users who trust FANUC’s reliable control and servo technology along with overall support for machine tools, can expect the same performance and value in general purpose motion control.

FANUC’s entire series of CRX collaborative robots are reliable, flexible, and can work for eight years without maintenance. Easy-to-use interactive programming allows operators to teach points using hand guidance or a Tablet TP with drag and drop icons.

FANUC CR-15iA Cobot Demonstrates Machine Tending

A CR-15iA collaborative robot mounted to a mobile cart will use iRVision® 3DV/400 to locate parts and efficiently load/unload a FANUC ROBODRILL.

FANUC’s ROBODRILL is a vertical machining center available in standard as well as advanced small, medium, and large models. The ROBODRILL offers versatility to handle a wide range of machining applications for large or small manufacturers.

FANUC has expanded the payload capacities of its CRX and CR cobot lines to handle products from 4 to 50kg. Now with 11 model variations, FANUC’s cobots work in a variety of industrial applications including assembly, inspection, material handling, packaging, palletizing, sanding, welding, and more.

High-Speed Tracking with FANUC SCARA Robot

The FANUC SR-3iA/U ceiling mount SCARA robot has a 3kg payload and 350 mm reach. Featuring a full 360-degree work envelope with no dead zones, the robot can access any point within its reach.

At CMTS, the SR-3iA/U will use iRVision 3DV and iRPickTool to pick various parts from a moving circular conveyor, move them to a 2D camera for inspection, then place them onto an outfeed conveyor into the appropriate Pass/Fail locations.

About FANUC Canada

FANUC Canada, located in Mississauga, Ontario, is a subsidiary of FANUC America Corporation. FANUC Canada provides industry-leading CNC systems, robotics and factory automation. FANUC’s innovative technologies and proven expertise help manufacturers maximize productivity, reliability and profitability.

FANUC embraces a culture of “Service First” which means that customer service is our highest priority. We are committed to supplying our customers with parts and support for the life of their FANUC products.

For more information, please call: 888-FANUC-US (888-326-8287) or visit our website: www.fanucamerica.com. Also, connect with us on YouTube, Twitter, Facebook, LinkedIn and Instagram.

FANUC America Corporation PR contact:

Robotics: Cathy Powell
Public Relations and Communications Manager
FANUC America Corporation
T: 248-377-7570
E: [email protected]

Factory Automation: Debra Schug
CNC Strategic Communications Specialist
T: 847.898.5673
E: [email protected]