FANUC America, the leading supplier of CNCs, robotics and ROBOMACHINEs will showcase its robot, cobot, and factory automation solutions at ATX West in Anaheim, CA, Feb. 6-8, in Booth #4500.
For Immediate Release
ROCHESTER HILLS, MI – (Jan. 9, 2024) – FANUC
America, a world leader in CNCs, robotics, and ROBOMACHINEs will showcase
its robot, cobot, and factory automation solutions at ATX West in Anaheim,
CA, Feb. 6-8, in Booth #4500.
CRX Cobot Demonstrations
Assembly with the Power
Motion i-Model A
– The CRX-10iA
cobot with the Power
Motion i-Model A (PMi-A)
will simulate brake rotor assembly. The PMi-A
moves
parts into position for the CRX, presses a simulated rivet into the part,
and performs quality inspection of the rivet press. FANUC's
Robot ON-SITE
enables the robot to control the functionality and actions through robotic
programming with the ability to “talk” to the CNC G-code program.
Palletizing - A CRX-25iA robot
with a 30kg payload
and 1,889mm reach will
demonstrate case palletizing. Guided by a 3DV/200 iRVision® sensor mounted
to the arm, the CRX-25iA will palletize boxes to
nearly 7’ high. In
addition, the CRX-25iA will be mounted to a mobile
cart to showcase its
flexibility. The robot can be easily repositioned by hand and uses vision to
automatically adjust to its new location and continue working accurately.
Easy Programming - A CRX-10iA
demo showcases the cobot’s
ease of use.
Attendees can try the cobot’s intuitive hand guidance and simple Tablet TP
programming with drag and drop icons.
FANUC’s series of CRX
collaborative robots all provide the utmost
reliability, flexibility, and can run for eight years without maintenance.
FANUC SCARA Robots
FANUC recently expanded its line of four-axis SCARA
robots to include the
SR-3iA/U ceiling mount featuring a full 360-degree
work envelope with no
dead zones, the robot can access any point within its reach. In addition,
FANUC’s SCARA lineup also includes the SR-3iA/C
and SR-6iA/C cleanroom
variants.
High-Speed Tracking - The SR-3iA/U ceiling mount
SCARA robot has a 3kg
payload and 350 mm reach. The SR-3iA/U will use
iRVision 3DV and iRPickTool
to pick various parts from a moving circular conveyor, move them to a 2D
camera for inspection, then place them onto an outfeed conveyor into the
appropriate Pass/Fail locations.
Packing Medical Vials - A
FANUC SR-12iA robot with the
Environmental Option
will pack and unpack trays of medical vials into a bin, and then pick up and
transfer a full bin to demonstrate the SR-12iA’s
payload capability. The
SR-12iA robot with the Environmental Option
includes white epoxy coating,
bellow covers, anti-rust bolts and seals, and an IP65 rating to withstand
dust and liquids.
FANUC MT-LINKi Optimizes Shop Floor
Connectivity
For machine shops looking to take advantage of IoT data, MT-LINKi provides
real-time equipment status and conditions info as well as other important
production and maintenance data.
MT-LINKi can monitor an entire factory and the
data can be viewed using web
browsers or a tablet device. Since MT-LINKi can
monitor various sensors
connected to machine tools, it is a simple way to bring a facility into the
IIoT universe.
Built-in Intelligence
FANUC offers application software for packaging and palletizing, integrated
iRVision® and tracking features, ROBOGUIDE
simulation, Dual Check Safety
(DCS), and Zero Down Time (ZDT) to help customers monitor and manage their
automation.
About FANUC America Corporation
FANUC America Corporation is a subsidiary of FANUC CORPORATION in
Japan, and
provides industry-leading CNC systems, robotics and ROBOMACHINEs.
FANUC’s
innovative technologies and proven expertise help manufacturers in
the
Americas maximize productivity, reliability and profitability.
FANUC America is headquartered at 3900 W. Hamlin Road, Rochester
Hills, MI
48309, and has facilities throughout North and South America. For
more
information, please call: 888-FANUC-US (888-326-8287) or visit our
website:
www.fanucamerica.com
. Also, connect with us on YouTube, Twitter,
Facebook,
LinkedIn and Instagram.
FANUC America Corporation PR contact:
Robotics: Cathy Powell
Public Relations and
Communications Manager
FANUC America Corporation
T:
248-377-7570
E:
[email protected]
Factory Automation: Debra Schug
CNC Strategic
Communications Specialist
T: 847.898.5673
E: [email protected]