Interested in a FANUC Product or Solution?

Contact us to receive more information on any product/solution, or to request a price quote. We'll be happy to answer any questions you may have, simply click below to get started.

Contact Us

FANUC America Press Releases

The latest news and product updates from the world's leading supplier of factory automation. For media inquiries, please email Public Relations.


FANUC America Demonstrates Cobot Palletizing at Pack Expo East

FANUC America, a world leader in CNCs, robotics, and ROBOMACHINEs will demonstrate its powerful CRX-25iA cobot palletizer at Pack Expo East in Philadelphia, March 18-20, in booth #1817.
by FANUC America | Feb 21, 2024

For Immediate Release

ROCHESTER HILLS, MI – (Feb. 21 2024) – FANUC America, a world leader in CNCs, robotics, and ROBOMACHINEs will demonstrate its powerful CRX-25iA cobot palletizer at Pack Expo East in Philadelphia, March 18-20, in booth #1817.

FANUC CRX-25iA Cobot is Ideal for Palletizing

At the show, a FANUC CRX-25iA cobot, offering an enhanced 30kg payload and 1,889mm reach will demonstrate case palletizing. Guided by a 3DV/200 iRVision® sensor mounted to the arm, the CRX-25iA will palletize boxes to nearly 7’ high. In addition, the CRX-25iA will be mounted to a mobile cart to showcase its flexibility. The robot can be easily repositioned by hand and uses vision to automatically adjust to its new location and continue working accurately.

FANUC’s entire series of CRX collaborative robots are reliable, flexible and can run for eight years without maintenance.

About FANUC America Corporation

FANUC America Corporation is a subsidiary of FANUC CORPORATION in Japan, and provides industry-leading CNC systems, robotics and ROBOMACHINEs. FANUC’s innovative technologies and proven expertise help manufacturers in the Americas maximize productivity, reliability and profitability.

FANUC America is headquartered at 3900 W. Hamlin Road, Rochester Hills, MI 48309, and has facilities throughout North and South America. For more information, please call: 888-FANUC-US (888-326-8287) or visit our website: www.fanucamerica.com . Also, connect with us on YouTube, Twitter, Facebook, LinkedIn and Instagram.

FANUC America Corporation PR contact:

Robotics: Cathy Powell
Public Relations and Communications Manager
FANUC America Corporation
T: 248-377-7570
E: [email protected]

Factory Automation: Debra Schug
CNC Strategic Communications Specialist
T: 847.898.5673
E: [email protected]