FANUC America, a pioneering force in automation, is set to unveil its latest lineup of robots, cobots, software, AI, and motion control innovations at Automate 2024 in Chicago. Visit FANUC in booth #1250 to see the future of industrial automation.
For Immediate Release
Rochester Hills, MI – (April 10, 2024) FANUC America,
a pioneering force in automation, is set to unveil its latest lineup of
robots, cobots, software, AI, and motion control innovations at Automate
2024 in Chicago. Visit FANUC in booth #1250 to see the future of industrial
automation.
“We’re excited to demonstrate our cutting-edge automation solutions at
Automate, said Lou Finazzo, Vice President, FANUC America. “Whether you’re a
start-up or a large-scale manufacturer, FANUC offers the world’s most
reliable and cost-efficient automation solutions. We are committed to
helping our customers achieve their production goals, enhance productivity,
and overcome labor constraints.”
CRX 30KG Cobot Demonstrations - Attendees will get a chance
to experience
FANUC’s wide range of CRX cobots and learn first-hand how easy it is to
program a CRX – even a 30kg model - using hand guidance or the intuitive
Tablet TP.
Collaborative Palletizing - A CRX-25iA food grade cobot
featuring a 30kg
payload and 1,889mm reach, will demonstrate collaborative palletizing. The
CRX picks boxes from an infeed conveyor and places to two pallets – stacking
the boxes to nearly 8’ high. The robot then depalletizes the boxes back to
the infeed conveyor, using its integrated force sensing capabilities to
ensure accurate placement.
The new food-grade
CRX-25iA cobot offers a robust
construction, corrosion
resistance, ease of cleaning, and compliance with food safety regulations to
provide a reliable and efficient solution for food companies. Designed to
operate safely in food processing facilities, the CRX-25iA’s white epoxy
coating meets the USDA Incidental Food Contact Requirements. In addition, it
has an IP67 washdown rating, and uses NSF H1 food grade lubricant.
The demonstration features the new PalletTool® 3, which enables operators to
create and modify unit loads directly from the Tablet TP with FANUC’s
PalletTool Turbo software using the newly updated user interface via
PalletTool 3. This new software package unlocks the ability to modify
systems quickly and easily on the floor without needing a PC.
Kitting - A CRX-10iA Food-Grade
option cobot will
demonstrate packing meat
and cheese gift boxes. Attendees are invited to try the cobot’s intuitive
hand guidance and easy-to-use Tablet TP.
Arc Welding - Lincoln Electric’s mobile welding cart
featuring FANUC’s
CRX-10iA offers attendees a hands-on programming
experience. The CRX welding
cobot is easy to program and use with the intuitive FANUC Tablet TP and the
ability to teach torch movements by hand. Lincoln Electric’s Power Wave R450
robotic welding platform provides the same industry-leading performance
found in traditional robotic welding.
Spot Welding – A CRX-20iA/L uses
iRVision® 3DV to locate
and pick parts of
different sizes from bins and place them onto a turntable. The table rotates
the parts to a FANUC R-2000iD/210FH robot equipped
with a Servo Gun. The
R-2000 robot simulates spot welding the parts together, and then parts
rotate back to the CRX to unload and return them to the bins. The
demonstration highlights how cobots can be used to assist industrial robots
with simple and repetitive tasks.
Gear Assembly - The CRX-5iA
cobot, featuring a 5kg payload
and 994mm reach
will pick and assemble small gears using integrated force control.
Vertical Put Wall - FANUC’s Power
Motion i Model A Plus
(PMi-AP) will move a
tool to random or user-specified locations on a put wall. Attendees can
choose which bins to get items from and then the tool pulls the sequence of
bins from the put wall and moves them to a conveyor belt for the CRX to
access the bin. When a wall bin arrives at the access point, a FANUC
CRX-10iA will pick an item and place it in an
order fulfillment bin. An
order is fulfilled once an item has been picked from each selected wall bin.
Once an order has been fulfilled, the put wall system will bring the bins
back to the CRX access point. The CRX then picks items from the order
fulfillment bin and places them back into the appropriate put wall bins
until each one has been restocked. Automated put walls are easy to deploy
and scale, helping warehouses and distribution centers improve productivity
by increasing order fulfillment, and decreasing labor costs.
The PMi-AP, which offers CNC-style motion control
for automated assembly and
other applications, integrates seamlessly into virtually any production
system using ethernet connection for easy communication between robots and
machines. Users who trust FANUC’s reliable control and servo technology
along with overall support for machine tools, can expect the same
performance and value in general purpose motion control.
Automated Palletizing/Depalletizing with FANUC M-710iD/50M
The new FANUC M-710iD/50M, combined with two
iRVision 3DV/1600 vision
sensors and the FANUC iPC, will use the iPC’s AI
Box Detection software to
locate boxes within stock carts. Once located, the M-710iD/50M will
depalletize boxes from one cart and utilize PalletTool to palletize them on
the opposite cart. Once a cart is empty, the process will be repeated by
depalletizing and palletizing back to the original stock cart. The tall
stock carts highlight the advantage provided by the M-710iD/50M’s curved
arm.
FANUC’s AI-driven iPC enables high-performance
advanced picking in
challenging lighting conditions to ensure seamless, reliable depalletizing.
iPC is a major benefit for this demonstration
because the boxes have
patterns that are difficult to segment and determine edge locations.
FANUC SCARA Solutions
FANUC recently expanded its line of four-axis SCARA
robots to include the
SR-3iA/U ceiling mount featuring a full 360-degree
work envelope with no
dead zones, the robot can access any point within its reach. In addition,
FANUC’s SCARA lineup also includes the SR-3iA/C
and SR-6iA/C cleanroom
variants.
High-Speed Tracking - The SR-3iA/U ceiling mount SCARA
robot has a 3kg
payload and 350 mm reach. The SR-3iA/U will use
iRVision 3DV and iRPickTool
to pick various parts from a moving circular conveyor, move them to a 2D
camera for inspection, then place them onto an outfeed conveyor into the
appropriate Pass/Fail locations.
Packing Medical Vials - A FANUC
SR-12iA robot
with the
Environmental Option
will pack and unpack trays of medical vials into a bin, and then pick up and
transfer a full bin to demonstrate the SR-12iA’s payload capability. The
SR-12iA robot with the Environmental Option includes
white epoxy coating,
bellow covers, anti-rust bolts and seals, and an IP65 rating to withstand
dust and liquids.
Cheeseburger Assembly - An LR Mate 200iD/7LC and SR-6iA/C –
both cleanroom
robots - will assemble cheeseburgers. First, the LR Mate 200iD/7LC uses
iRVision 3D to pick and place four hamburger buns
on one of two slides. The
SR-6iA/C SCARA robot will then pick and place a
hamburger patty and a piece
of cheese on top of each bun. The LR Mate completes the cheeseburgers by
placing a tomato slice and a top bun (the robots alternate between placing
items on each slide). Once all four cheeseburgers are completed, the robots
remove items in reverse order and the cycle repeats.
The popular LR Mate 200iD series of tabletop industrial robots
offers a
“best in class” work envelope for both upright and invert mount
installations. Ten models include clean room and wash proof versions, each
with various wrist speeds and reaches to accommodate even the most limited
workspace. The LR Mate series, introduced over 30 years ago, is one of
FANUC’s most popular robot models with more than 70,000 units installed
globally.
The SR-6Ai/C SCARA has a 6kg payload and 650 mm reach. It
features a white
epoxy coating and is rated IP54, meaning it is protected against
contamination from limited amounts of dust and other particles as well as
water spray. The SR-6iA/C can meet ISO Class 2 to ISO Class 5 for
cleanroom
operation and uses NSF-H1 food-grade grease and anti-rust bolts for food
handling applications.
Visual Line Tracking – A FANUC LR
Mate uses an overhead
mounted 3DV/400
iRVision Sensor and Line Tracking with iRPickTool to find and track candy
moving down a conveyor. The robot picks a part and places it into a bin. The
system highlights the speed and accuracy of the 3DV/400 vision sensor and
the ability to detect the 3D orientation of a work piece on a noisy
background.
FANUC MT-Linki Optimizes Shop Floor Connectivity
For machine shops looking to take advantage of IoT data, MT-Link
i provides
real-time equipment status and conditions info as well as other important
production and maintenance data. Since MT-LINKi can monitor various sensors
connected to machine tools, it is a simple way to bring a facility into the
IIoT universe.
Built-in Intelligence
FANUC offers application software for packaging and palletizing, integrated
iRVision® and tracking features, ROBOGUIDE
simulation, Dual Check Safety
(DCS), and Zero Down Time (ZDT) to help customers monitor and manage their
automation.
Learn from FANUC’s subject matter experts at Automate in the following
conference sessions. For more information visit Automate’s Conference Agenda
Page.
About FANUC America Corporation
FANUC America Corporation is a subsidiary of FANUC CORPORATION in
Japan, and
provides industry-leading CNC systems, robotics and ROBOMACHINEs.
FANUC’s
innovative technologies and proven expertise help manufacturers in
the
Americas maximize productivity, reliability and profitability.
FANUC America is headquartered at 3900 W. Hamlin Road, Rochester
Hills, MI
48309, and has facilities throughout North and South America. For
more
information, please call: 888-FANUC-US (888-326-8287) or visit our
website:
www.fanucamerica.com
. Also, connect with us on YouTube, Twitter,
Facebook,
LinkedIn and Instagram.
FANUC America Corporation PR contact:
Robotics: Cathy Powell
Public Relations and
Communications Manager
FANUC America Corporation
T:
248-377-7570
E:
[email protected]
Factory Automation: Debra Schug
CNC Strategic
Communications Specialist
T: 847.898.5673
E: [email protected]