Interested in a FANUC Product or Solution?

Contact us to receive more information on any product/solution, or to request a price quote. We'll be happy to answer any questions you may have, simply click below to get started.

Contact Us

FANUC America Press Releases

The latest news and product updates from the world's leading supplier of factory automation. For media inquiries, please email Public Relations.


A New Era of FANUC’s ROBODRILL Vertical Machining Center with More Offerings than Ever

The new FANUC ROBODRILL α-D28LiB5ADV Plus Y500 features a larger table, more tools, new capabilities, all in the same space-saving footprint.
by FANUC America | Aug 27, 2024

ROCHESTER HILLS, MI – (August 27, 2024) – FANUC America, a global industrial automation leader, unveils the latest addition to FANUC’s ROBODRILL vertical machining center (VMC) lineup, the new α-D28LiB5ADV Plus Y500. This new VMC offers more advantages to any production machine shop by featuring a larger table, shorter drilling and tapping cycles as well as more tools coupled with faster tool changes. FANUC America will be introducing the new ROBODRILL α-D28LiB5ADV Plus Y500 at the 2024 International Manufacturing Technology Show in Chicago, IL., Sept. 9-14 in booth S-338919.

FANUC’s ROBODRILL α-D28LiB5ADV Plus Y500 is designed for peak performance covering a wide range of tasks and excelling at machining large workpieces. This is due to its extended Y-axis stroke (500 mm) and increased table size, all without increasing the ROBODRILL’s footprint. The new ROBODRILL speeds up drilling and tapping operations via a rapid Z-axis acceleration (2.2 G) and traverse rate (60m/min). Plus, with an expanded tool capacity of 28 tools and lightning-fast changes, the new ROBODRILL α-D28LiB5ADV Plus Y500 will boost productivity for any machining application.

“We understand modern machine shops, particularly in the automotive industry, need to produce constantly, maximize machine time, and reduce any interruptions to production,” says Lou Finazzo, Vice President of FANUC America. “The new α-D28LiB5ADV Plus Y500 is built for reliable production, tailored to our customers’ needs for extra capabilities without sacrificing any floorspace.”

The enhanced performance of the new ROBODRILL α-D28LiB5ADV Plus Y500 is designed to help machine shops drive down cycle times with faster speeds and improved productivity. Additionally, with easy robotic integration tools with FANUC robots, automating machine tending is a breeze with FANUC ROBODRILL Plus.

This newest ROBODRILL Plus continues to build on ROBODRILL’s over 50-year reputation as the most reliable VMC with industry-leading uptime. The ROBODRILL Plus lineup offers precision and versatility with three model sizes available each in two choices: Standard or Advanced. With nearly a half million operating around the world, FANUC ROBODRILLs are popular for not only their performance, but 24/7 local support available to keep all machine shops running all the time.

For more information, please visit https://www.fanucamerica.com/products/robodrill.

About FANUC America Corporation

FANUC America Corporation is a subsidiary of FANUC CORPORATION in Japan, and provides industry-leading CNC systems, robotics, and factory automation.  FANUC’s innovative technologies and proven expertise help manufacturers in the Americas maximize productivity, reliability, and profitability. 

FANUC America is headquartered at 3900 W. Hamlin Road, Rochester Hills, MI 48309, and has facilities throughout North and South America.  For more information, please call: 888-FANUC-US (888-326-8287) or visit our website: https://www.fanucamerica.com. Also, connect with us on YouTube, X, Facebook, LinkedIn and Instagram

 

FANUC America Corporation Factory Automation, ROBODRILL, IoT and Paint PR contact:

Debra Schug
FANUC America PR-Content Lead, Factory Automation, ROBODRILL, Paint
[email protected]