FANUC America will demonstrate its latest ROBODRILL Plus Vertical Machining Center and CRX Cobot at Performance Racing Industry, Dec. 12-14 in Indianapolis, booth #5659
ROCHESTER HILLS, MI – (December 3, 2024)
–
FANUC America, the world leader in CNCs, robotics, and ROBOMACHINEs, will
demonstrate its high-performance vertical machining centers as well as
easy-to-use welding collaborative robots at the Performance Racing Industry
(PRI) Show, Dec. 12-14 in Indianapolis, in booth #5659.
FANUC ROBODRILL Plus Vertical Machining Center
FANUC’s ROBODRILL
α-DiB5 Plus vertical machining center comes available
in
three sizes (small, medium, and large) to accommodate a wide range of
production operations. The ROBODRILL DiB5 Plus provides customers
with
unrivaled quality and precision features. A compact design with
accessibility from all sides enhances overall efficiency for high-speed
milling, drilling, and tapping applications.
Powered by the FANUC
Plus Series 31i-B5 Control, the ROBODRILL DiB5 Plus
provides unbeatable cycle times, tool change times as fast as 0.7 seconds,
and a servo-driven turret capable of handling tools weighing up to 4 kg.
Because FANUC products share common servo and control platforms, the
ROBODRILL Plus is easy to use as well as integrate FANUC robots for any
automated machine tending application.
At PRI, FANUC’s ROBODRILL Plus will be featured in two automated
processes,
including:
High-Speed Impeller Machining
A FANUC ROBODRILL α-D14SiB5 Plus will showcase
high-efficiency
machining of
aluminum automotive impellers. The ROBODRILL will be equipped with a
Nikken
BF3 for fast 5-axis simultaneous operations delivering an extremely
high-quality finish.
High-Efficiency Steel Machining
A FANUC ROBODRILL α-D21MiB5 ADV Plus paired with the
DDR-TiB will
demonstrate high-speed 4-axis milling, drilling, and tapping on a
block of
steel. This application highlights the ability of the ROBODRILL Plus
to
perform multi-axis, heavy steel milling applications without
sacrificing
speed or capability.
Easy-to-Use CRX Cobot
FANUC’s collaborative robots are easy to use and flexible solutions for
companies looking to improve productivity and solve labor issues.
FANUC’s
entire series of CRX
collaborative robots are reliable, flexible, and can
work for up to eight years without maintenance.
At PRI, FANUC’s CRX-10iA/L will simulate easy welding with
hands-on
demonstrations that showcase the intuitive programming of FANUC’s new
cobot
wrist buttons.
Connected Technologies
FANUC’s MT-Linki
IoT offering allows robotics and machine tool
users the
ability to use advanced analytics to drive smarter, faster business
decisions for industrial companies. We’ll be showing how
MT-Linki
connects
all the FANUC equipment in our own booth and the insights it provides.
About FANUC America Corporation
FANUC America Corporation is a subsidiary of FANUC CORPORATION in Japan, and
provides industry-leading CNC systems, robotics and factory automation.
FANUC’s innovative technologies and proven expertise help
manufacturers in
the Americas maximize productivity, reliability and profitability.
FANUC America is headquartered in Rochester Hills, MI and has facilities
throughout North and South America. For more information, please call:
888-FANUC-US (888-326-8287) or visit our website: www.fanucamerica.com.
Connect with us on YouTube, X,
Facebook,
LinkedIn
and
Instagram.
FANUC America Corporation PR Contact:
[email protected]