Interested in a FANUC Product or Solution?

Contact us to receive more information on any product/solution, or to request a price quote. We'll be happy to answer any questions you may have, simply click below to get started.

Contact Us

FANUC America Press Releases

The latest news and product updates from the world's leading supplier of factory automation. For media inquiries, please email Public Relations.


FANUC Expands Line of High-Performance SCARA Robots

FANUC has expanded its line of high-performance SCARA ROBOTS, offering more reach and payload options to companies with assembly, packaging, pick and place, and inspection processes.
by FANUC America | May 11, 2021

More Options to Help Companies Achieve Their Production Goals

For Immediate Release

ROCHESTER HILLS, MI – (MAY 11, 2021) – FANUC America, the leading supplier of CNCs, robotics, and ROBOMACHINEs has expanded its line of high-performance SCARA ROBOTS, offering more reach and payload options to companies with assembly, packaging, material handling, and inspection processes.       

FANUC’s family of 4-axis SCARA robots has grown to include the SR-3iA, SR-6iA, SR-12iA, and new SR-20iA models with 3kg, 6kg, 12kg and 20kg payload capacities, and a 400-1,100mm reach, respectively. 

The small SR-3iA and SR-6iA SCARAs have a compact footprint and space-saving design for maximum efficiency.   In addition, the SR-3iA/H and SR-6iA/H are 3-axis variants that provide strong performance and an affordable alternative to small linear slide products.  The higher-payload SR-12iA and SR-20iA provide flexibility with a large vertical stroke, and an environmental option for harsh conditions.  All of FANUC’s SCARA robots include superior robot motion, high-speed operation and ultimate precision.

“FANUC’s SCARA robots provide great solutions when speed and repeatability are essential,” said Eric Potter, director of FANUC’s general industry and automotive engineering segments.  “Our SCARA robots are designed to help customers increase productivity in a number of industries including consumer electronics, auto components, plastics, food & beverage, lab automation, appliances and medical device manufacturing.” 

Powered by the R-30iB Compact Plus controller, FANUC’s SCARA robots have the same intelligence and reliability that’s available on all FANUC robots, including integrated iRVision®, conveyor tracking (iRPickTool), and most other software options.  FANUC’s latest SCARA iRProgrammer user interface makes it easy to setup and program the robot on a Tablet or PC (Teach Pendant is optional).

“With over 715,000 robots installed globally, FANUC is a household name in manufacturing.  Now, with our expansive line of SCARAs we’re able to help more companies solve their manufacturing issues,” added Potter.

FANUC SCARA Robot Features and Benefits                                                                       

- Space-saving design minimizes interference with peripheral devices. The SR-3iA and SR-6iA have an ultra-compact footprint and slim profile.  The SR-12iA and SR-20iA have internal cable routing to eliminate interference. 

- Six models available: SR-3iA (4-axis/400mm reach), SR-3iA/H (3-axis/400mm reach), SR-6iA (4-axis/650mm reach), SR-6iA/H (3-axis/650mm reach), SR-12iA (4-axis/900mm reach), and the SR-20iA (4-axis/1,100mm reach).

- The SR-12iA and SR-20iA offer environmental options including white epoxy coating, bellow covers, anti-rust bolts and seals, and IP65 rating to withstand dust and liquids.

- SR-12iA and SR-20iA provide high inertia and high payloads, maximizing flexibility to handle large work pieces.

- Highest motion performance with continuous fast operation at all payloads.

- A generous vertical stroke makes it possible to perform assembly, packaging and various handling operations.

- Bottom cable exit (optional) protects cables, and saves valuable floor space for higher efficiency.

- Brake release switch on the robot’s arm allows easy error recovery.

- High-performance R-30iB Compact Plus controller requires minimal space and allows layout and installation flexibility.

- Web-based iRProgrammer user interface for intuitive and easy robot setup and programming on a PC or Tablet (Teach Pendant is optional).

- Standard CE/NRTL compliance on the R-30iB Compact Plus controller allows global deployment without any additional cost.

- Same high performance intelligent software options across the entire FANUC robot line, including iRVision (integrated vision), conveyor tracking (iRPickTool), fieldbus connectivity and integrated safety.

For more information about FANUC’s SCARA robots visit:  www.fanucamerica.com/scara.

About FANUC America Corporation

FANUC America Corporation is a subsidiary of FANUC CORPORATION in Japan, and provides industry-leading CNC systems, robotics and factory automation.  FANUC’s innovative technologies and proven expertise help manufacturers in the Americas maximize productivity, reliability and profitability. 

FANUC embraces a culture of “Service First” which means that customer service is our highest priority.  We are committed to supplying our customers with parts and support for the life of their FANUC products.   

FANUC America is headquartered at 3900 W. Hamlin Road, Rochester Hills, MI 48309, and has facilities in:  Auburn Hills, MI; Atlanta; Boston; Charlotte; Chicago; Cincinnati; Cleveland; Houston; Huntington Beach, CA; Los Angeles; Minneapolis; Montreal; Pine Brook, NJ; Pontiac, MI; Birmingham, AL; San Francisco; Seattle; Toronto; Buenos Aires, Argentina; Sao Paulo, and Manaus, Brazil; and Aguascalientes, Monterrey, and Queretaro, Mexico.  For more information, please call: 888-FANUC-US (888-326-8287) or visit our website: www.fanucamerica.com.  Also, connect with us on YouTube, Twitter, Facebook, LinkedIn and Instagram

FANUC America Corporation PR contact:

Robotics: Cathy Powell
Public Relations and Communications Manager
FANUC America Corporation
T: 248-377-7570
E: [email protected]

Factory Automation: Debra Schug
CNC Strategic Communications Specialist
T: 847.898.5673
E: [email protected]

                                                                ###