FANUC will showcase our latest automation solutions to help drive the future of manufacturing at FABTECH 2021 in Chicago, Ill.
ROCHESTER HILLS, MI – (Sept. 2, 2021) – FANUC
America, the leading supplier of CNCs, robotics, and ROBOMACHINEs will
showcase our latest automation solutions to help drive the future of
manufacturing at FABTECH 2021 in Chicago, Ill. See us
in booth #B23022 in the North Hall, and booth #D45535 in the East
Hall’s painting pavilion.
Factory Automation Demonstrations
FANUC’s Factory Automation division will demonstrate Visual Twin and
Additive Manufacturing at FABTECH. The Visual Twin demonstration offers an
exciting new way to see part production while highlighting FANUC’s
end-to-end digitalization solutions for the machine shop. FANUC’s Visual
Twin is an exact software replica of real CNC machine tools.
The Visual Twin will display a virtualized 5-axis machine tool cutting a
part, which mirrors the real-world machine’s behavior.
Additive Manufacturing, otherwise known as 3D printing, has been gaining
popularity in industrial manufacturing to create prototypes, tooling and
end-use production parts. Applications, including medical implants and
aerospace parts, are growing as new hybrid machine tools combine additive
manufacturing with CNC machining. The new demo highlights
FANUC’s capabilities in this burgeoning market by incorporating a
3-axis machine equipped with a four-extruder head into a plastic 3D printer.
FANUC 30i-B CNC equipped with the
21.5” Panel i H Pro will be featured on the machine to demonstrate its
custom slicing and post-processing capabilities.
Robotic Demonstrations
Adaptive Arc
Welding: A collaborative robot system will
demonstrate how to help welding customers address gap conditions.
First, an operator loads coupons and sets variable gaps of 0-1.5mm between
the work pieces. Next, a CR-15iA collaborative robot uses
FANUC’s Seam Tracking software with SERVO ROBOT’s FUJI-CAM 2.0
sensor to communicate the gap conditions to the robot, which then performs
adaptive welding. The adaptive process has the ability to change
weaving amplitude, weave frequency, travel speed, wire feed speed, trim, as
well as positional bias in X,Y,Z directions.
The demonstration also features the Lincoln Electric Power Wave® R450
robotic power source with the Advanced Module using the GMAW Pulse
process.
CRX Collaborative Arc
Welding Robot:
FANUC’s CRX collaborative arc welding robot offers the
same high level of performance that FANUC ARC Mate robots are known for
including the latest technologies and world-renowned reliability.
Built-in sensors on each axis can allow the CRX welding cobot to work safely
alongside people without the need for expensive guarding. In addition,
the CRX can operate for eight years maintenance-free, which is a major
advantage for companies looking to lower costs and increase
productivity.
The CRX is extremely easy to use – even for those who have never used a
robot. Interactive programming allows operators to teach weld joints
using hand guidance or a new tablet interface with drag and drop
icons. The CRX welding cobot supports several of FANUC’s
advanced features including iRVision, Torch Angle Control, Touch
Sensing and Thru Arc Seam Tracking (TAST). The CRX is shown with
Lincoln Electric’s Power Wave® R450 robotic power source, and the
new Lincoln Electric Smart Torch. FANUC’s CRX welding cobot
demonstration will allow visitors to try its easy hand guidance and tablet
programming features.
In addition, Lincoln Electric’s Fab-Pack® Cobot
Guru™> featuring FANUC’s CRX will offer attendees a
hands-on experience of this new collaborative robot welding
solution.
The Fab-Pak Cobot Guru robotic welding system includes simplified programming
with the new CRX tablet-based teach pendant, and the ability to teach at the
torch by hand. Built for the industrial space, the Fab-Pak Cobot Guru
system is compatible with all of Lincoln Electric’s weld programs to
help customers maximize productivity.
Painting:
FANUC America has designed and built its painting robots at the company’s
Rochester Hills, Mich., headquarters for nearly 40 years. The FANUC
P-40iA is the latest in the paint robot series. Ideal for a
variety of painting and coating applications, the six-axis P-40iA
offers the same reliability and proven technology as all FANUC
products.
At Fabtech, a P-40iA paint robot equipped with
the R-30iB Plus Mate controller will demonstrate painting metal
parts using coordinated motion to reach all surfaces of the
parts. Visitors will also have the opportunity to try out the
new “Easy Teach” hand-guidance programming feature.
In addition to being easy to use, the P-40iA robot is extremely
flexible to accommodate small lot sizes, new styles and other modifications,
providing customers an affordable and versatile solution. Slim and
lightweight, the P-40iA robot offers a variety of mounting
positions, which helps companies challenged with small and narrow
workspaces.
Spotwelding:
The R-2000iD/210FH spot welding
robot is the latest model in a large family of industrial
robots offering a variety of payloads and reaches. The robot offers a
compact design with a hollow arm for better cable management, which
minimizes interference with system equipment and allows the robot to operate
in tight workspaces. Featuring a 210kg payload and 2605mm reach, the
R-2000iD/210FH is ideal for spot welding and material handling
applications.
At the show, the R-2000iD/210FH robot equipped with integrated FANUC
Servo Gun Control and a hollow arm for spot welding dress out will perform
simulated spot welding in and around a truck cab. The robot will use
Dual Check Safety (DCS) Speed and Position Check software to limit the
robot’s envelope within the compact workspace. Also featured
will be FANUC’s latest R-30iB Plus controller with an
intuitive iPendant for easy setup and operation.
FANUC will participate in two technology sessions including:
F34: Laser Ecosystems for Fiber
Laser Cutting & Surface Cleaning on Tuesday,
September 14, 8:00 -9:30 AM. Michael Sharpe, Laser Business Development
Manager to present: Laser Ecosystem - Dynamics Through Full
Digital Control.
F202: Automation for Metal
& Finishing Processes on Wednesday, September 15,
3:30 - 5:00 PM. Barton Faylor, Senior Industry Marketing/Program
Manager to present: CAD to Path Robot Programming. Is it Myth
or Reality?
For more information on FANUC’s presence at FABTECH, visit www.fanucamerica.com/fabtech.
About FANUC America Corporation
FANUC America Corporation is a subsidiary of FANUC CORPORATION in Japan, and
provides industry-leading CNC systems, robotics and factory
automation. FANUC’s innovative technologies and proven expertise
help manufacturers in the Americas maximize productivity, reliability and
profitability.
FANUC embraces a culture of “Service
First” which means that customer service is our highest
priority. We are committed to supplying our customers with parts and
support for the life of their FANUC products.
FANUC America is headquartered at 3900 W. Hamlin Road, Rochester Hills, MI
48309, and has facilities in: Auburn Hills, MI; Atlanta; Boston;
Charlotte; Chicago; Cincinnati; Houston; Huntington Beach, CA; Los Angeles;
Minneapolis; Montreal; Pine Brook, NJ; Pontiac, MI; Birmingham, AL; San
Francisco; Seattle; Toronto; Buenos Aires, Argentina; Sao Paulo, and Manaus,
Brazil; and Aguascalientes, Monterrey, and Queretaro, Mexico. For more
information, please call: 888-FANUC-US (888-326-8287) or visit our website:
www.fanucamerica.com . Also, connect with
us on YouTube, Twitter, Facebook,
LinkedIn and Instagram.
FANUC America Corporation PR contact:
Robotics: Cathy Powell
Public Relations and Communications
Manager
FANUC America Corporation
T: 248-377-7570
E: [email protected]
Factory Automation: Debra Schug
CNC Strategic Communications
Specialist
T: 847.898.5673
E: [email protected]
###