By using this site, you agree to our updated Legal Terms and Privacy Policy
Contact us any time and we'll make sure that you receive the support you need. We're happy to answer any questions you may have, simply click below to get started.
We're here to meet your needs. Contact us today.
Contact us
FANUC products are renowned for the reliability and longevity and often times outlive the original production process they were intended for. FANUC has helped manufactures redeploy robots for new application by providing a comprehensive robot evaluation by our team of experts. Through extensive testing of components and parts that receive extensive wear, our engineers formulate a reconditioning plan to restore your robot to OEM specification and offer a full one-year-warranty.
FANUC America Corporation is the only certified repair house for your robots and exclusively offers our FANUC Certified Repair Certification on all recertified robots.
Our Certified Robot Reapplication Group offers a wide range of services that include the following:
Ask about our robot enhancement and reapplication services, today!
FANUC America’ robot evaluation service includes a thorough examination to determine the condition of the robot(s). We identify any areas that do not meet original factory specifications using a multitude of factory authorized tests. FANUC America will provide an updated proposal outlining the recommended repairs and maintenance services required to bring the robot back to OEM specifications.
Robot Evaluation Service consists of:
To learn more about our robot evaluation services or to get a quote, contact crcsales@fanucamerica.com, or fill out the contact us form below.
The re-certification service uses the evaluation results to bring your robot back to OEM specifications. The service includes complete disassembly of each axes or assemblies that did not pass the tests performed during the robot evaluation. The intent of this process is to further identify any non-conforming items which may otherwise be difficult to detect. The re-certification service will correct all non-conformities identified. Testing and validation is performed to ensure that the robot(s) meet original factory specifications.
Re-Certification Service consists of four processes:
The exclusive process will bring your robot back to original factory specifications using the latest engineering information and processes available only from FANUC America. This robot reapplication service is backed by the industry’s best warranty*.
*Robots that undergo the robot reapplication service process including all repairs deemed necessary by FANUC America include a full, one-year, parts and labor warranty. Any services conducted short of the outlined robot reapplication service will receive a standard 1 year parts and labor on only the parts replaced by FANUC America.
This service is recommended for robots that have been in production for over 31,000 hours. This service would consist of a complete overhaul of the robot which entails replacement of the wrist, cable set, all motors, and all RVs. FANUC America does not generally recommend a complete overhaul due to the prohibitive cost. The robot restoration service will bring the robot back to FANUC factory standard specifications and once completed will result in a full one-year robot warranty.
Sometimes the application you purchased the robot for changes. Instead of purchasing a new robot, let our FANUC Certified Robot Reapplication repurpose it, by converting hardware and or software the robot to meet your new application needs. Contact us at crcsales@fanucamerica.com, or fill out the contact us form below to discuss your changing application. We will need the F# of the robot and if possible the F# of a robot that already has the desired hardware and software.
FANUC offers on site evaluations and refurbishments for customers that do not have the option to send their robots to FANUC due to production needs or accessibility.
Evaluations:
FANUC America’s onsite evaluation services are similar to what is included with our services we provide at our facility. A thorough examination to determine the condition of the robot(s). We identify any areas that do not meet original factory specifications using a multitude of authorized tests. FANUC America will provide an proposal outlining the recommended repairs and maintenance services required to bring the robot back to OEM specifications.
Onsite Evaluations differences:
Refurbishments:
FANUC America will refurbish your robots based on evaluation results, we will bring you robots back to OEM standards to improve/maintain quality and uptime. For example, customers may need replace wear items such as cables and paint lines that route through robot catracks. The work can be completed during production downtime windows such as weekends and holidays. FANUC has a dedicated team that will work with you to develop an action plan based on your available downtimes.
*Robot refurbishment service will receive a standard 1 year parts and labor warranty on all parts replaced by FANUC America.
FANUC offers several robot options that can be purchased with the initial robot purchase or they can be purchased aftermarket and can be installed on your robot by our Certified Robot Reapplication technicians. These options that weren’t originally purchased with the robot, such as iRVision enhance your robots capability and can improve the overall application.
To learn more about our robot customization services or to get a quote, contact crcsales@fanucamerica.com, or fill out the contact us form below.