iRVision-2D Operation and Programming
Course Code: iRvision-2D-R30iA
2 DAYS / 16 HOURS
This course covers the basic areas and procedures required for an operator, technician, or programmer to configure, teach, test, and modify iRVision applications on R-30iA controllers.
Objetivos del Curso:
- Turn on and move the robot
- Set up communication between the robot and the teaching computer
- Configure and calibrate the camera
- Teach a vision process (stationary camera)
- Teach a vision process (camera mounted on the robot)
- TPP Programming
- Common faults and alarms
Audience
This course is designed for people who need to install, configure, program, or troubleshoot a FANUC iR-Vision system.
Prerequisites
Programming and Operation of Software Handling Tool, Spot Tool, Arc Tool or Dispense Tool.
Complete Description
The course consists of theoretical exposition in the classroom, demonstrations, practical exercises, designed to reinforce learning.
Exam Note
In order to identify the level of initial knowledge and achievement during the course, an exam is applied at the beginning of the course and another at the end.
Security Note
All exercises performed during the course include recommended safety procedures.
Teaching Materials
La documentación y material didáctico se entrega en idioma inglés.