FANUC America will feature factory automation and robotic manufacturing solutions at Eastec, Oct. 19-21 in Springfield, MA in booth #1714, and Southtec, Oct. 26-28 in Greenville, SC in booth #2129.
For Immediate Release
ROCHESTER HILLS, MI – (OCTOBER 7, 2021) – FANUC America, the leading supplier of CNCs, robotics, and ROBOMACHINEs will feature factory automation and robotic manufacturing solutions at Eastec, Oct. 19-21 in Springfield, MA in booth #1714, and Southtec, Oct. 26-28 in Greenville, SC in booth #2129.
Easy-to-Use CRX Collaborative Robot
FANUC’s latest CRX collaborative robot offers the same high level of performance that all FANUC products are known for including the latest technologies and world-renowned reliability. It supports several of FANUC’s advanced features including iRVision, and is a perfect fit for any application where collaborative robots can help customers achieve higher efficiencies. Also, interactive programming enables users to teach points using hand guidance or a new tablet interface with drag and drop icons.
The CRX cobot is an easy-to-use and flexible solution for a variety of applications, including machine tending, inspection, welding and more. Built-in sensors on each axis can allow the CRX cobot to work safely alongside people without the need for expensive guarding. In addition, the CRX can operate for eight years maintenance-free, which will help companies reduce costs and maximize productivity.
At both Eastec and Southec, attendees will be able to try the CRX Cobot’s easy hand guidance and intuitive tablet programming features.
Click here to watch the FANUC CRX working in a variety of manufacturing environments.
Factory Automation Demonstrations
Attendees at both Eastec and Southec will have the opportunity to experience a new and exciting way to see part production. Our Visual Twin demonstration highlights FANUC’s end-to-end digitalization solutions for the machine shop. By seamlessly working with various machine tool builders as well as Mastercam and ModuleWorks, FANUC’s Visual Twin is an exact software replica of real CNC machine tools. The Visual Twin will display a virtualized 5-axis machine tool cutting a part, which mirrors the real-world machine’s behavior.
Also from the Factory Automation division, we are demonstrating the seamless integration and high performance of FANUC’s CNC and servo systems in a Laguna iQ desktop CNC router. Equipped with a complete FANUC CNC system, the display shows how well the machine, control and drives all work together to bring unbeatable value in reliability and accuracy. The simulator may also be used for learning servo parameter setup and enhance servo motor tuning skills.
FANUC LR Mate 200iD Tabletop Robot
At the Eastec show, a FANUC LR Mate 200iD robot will use FANUC iRVision to locate 3D-printed letters on a small tray, then pick and place them in random locations. Next, the robot moves the tray to the opposite side and replaces the letters. Finally, the robot traces each letter with a laser pointer to demonstrate ROBOGUIDE’s CAD-to-Path function.
FANUC’s popular LR Mate 200iD series of tabletop industrial robots make ideal additions to any small or medium shop looking to automate their process. The LR Mate 200iD robot offers a “best in class” work envelope for both upright and invert mount installations. Ten models include clean room and wash proof versions, each with various wrist speeds and reaches to accommodate even the most limited workspace. Since the LR Mate series was launched nearly 30 years ago, it has become one of FANUC’s biggest sellers, with over 70,000 units installed across the globe.
High-Speed SCARA Robot
At the Southtec show, a FANUC SR-3iA SCARA robot will use iRVision to pick up letters from both sides of a part nest, and slide them into a fixture to spell out “SR3 ZDT.” The demonstration highlights the advantages of using FANUC’s iRVision to locate parts, and reorient them on the fly.
FANUC’s family of 4-axis SCARA robots has grown to include the SR-3iA, SR-6iA, SR-12iA, and new SR-20iA models with 3kg, 6kg, 12kg and 20kg payload capacities, and a 400mm - 1100mm reach, respectively. FANUC’s SCARA robots are designed to help customers increase productivity in a number of industries including consumer goods, batteries and other auto components, plastics, lab automation, appliances and medical devices.
The small SR-3iA and SR-6iA SCARAs have a compact footprint and space-saving design for maximum efficiency. In addition, the SR-3iA/H and SR-6iA/H are 3-axis variants that provide strong performance and an affordable alternative to small linear slide products. The higher-payload SR-12iA and SR-20iA robots provide flexibility with a large vertical stroke, and an Environmental Option for harsh conditions. All of FANUC’s SCARA robots provide excellent robot motion, speed and precision.
Powered by the R-30iB Compact Plus controller, FANUC’s SCARAs have the same intelligence and reliability that’s available on all FANUC robots, including integrated iRVision®, conveyor tracking (iRPickTool), and most other software options. FANUC’s SCARA iRProgrammer user interface makes it easy to setup and program the robot on a Tablet or PC (Teach Pendant is optional).
About FANUC America Corporation
FANUC America Corporation is a subsidiary of FANUC CORPORATION in Japan, and provides industry-leading CNC systems, robotics and factory automation. FANUC’s innovative technologies and proven expertise help manufacturers in the Americas maximize productivity, reliability and profitability.
FANUC embraces a culture of “Service First” which means that customer service is our highest priority. We are committed to supplying our customers with parts and support for the life of their FANUC products.
FANUC America is headquartered at 3900 W. Hamlin Road, Rochester Hills, MI 48309, and has facilities in: Auburn Hills, MI; Atlanta; Boston; Charlotte; Chicago; Cincinnati; Houston; Huntington Beach, CA; Los Angeles; Minneapolis; Montreal; Pine Brook, NJ; Pontiac, MI; Birmingham, AL; San Francisco; Seattle; Toronto; Buenos Aires, Argentina; Sao Paulo, and Manaus, Brazil; and Aguascalientes, Monterrey, and Queretaro, Mexico. For more information, please call: 888-FANUC-US (888-326-8287) or visit our website: www.fanucamerica.com. Also, connect with us on YouTube, Twitter, Facebook, LinkedIn and Instagram.
FANUC America Corporation PR contact:
Robotics: Cathy Powell
Public Relations and Communications Manager
FANUC America Corporation
T: 248-377-7570
E: [email protected]
Factory Automation: Debra Schug
CNC Strategic Communications Specialist
T: 847.898.5673
E: [email protected]
###