Interested in FANUC CNC Retrofit Solution?

Contact us to receive more information on any CNC retrofit solution, or to request a price quote. We'll be happy to answer any questions you may have, simply click below to get started.

Contact Us
CNC retrofit

CNC Retrofits: Extend the lifespan of your machine tools with a new FANUC control system

Retrofitting an aging CNC system with a new FANUC CNC will save long term costs and boost the machine’s productivity while adding to the uptime, reliability and efficiency. A CNC retrofit with FANUC’s products can help businesses meet changing manufacturing requirements and customers’ evolving demands.

Request A Quote

CNC Retrofit

Find your CNC Retrofit Solution

Interested in CNC retrofitting your legacy machine tool, but not sure where to start? Download FANUC America’s CNC Retrofit App! This app will help you collect and submit relevant information about your equipment and how to go about retrofitting it with FANUC products.

Download on the App Store Get it on Google Play

What is a CNC retrofit?

A CNC retrofit upgrades the control system, the servo and spindle motors, the motor amplifiers, cables and I/O units including the operator’s panel.

Aerospace Skin Milling

Production Benefits from Retrofitting

Learn more about how Microtrol Engineering helped retrofit Cincinnati skin mills with new FANUC controls, motors and drives to boost quality and efficiency. “I always recommend FANUC,” says Brandt Fine, president of Microtrol Engineering. “FANUC is a solid platform. I install, and I don't have to worry about it breaking down.”

View Case Study
cnc retrofitting

Retrofitting to Stay Competitive

Learn more about how FANUC and Fives helped Lincoln Park Boring Company achieve more efficiency, shorter production times and the ability to go after new business with a CNC retrofit.

View Case Study
b&k cnc retrofitting

Standardizing with FANUC Controls

FANUC controls give machine tool builder and retrofitter Bourn & Koch the flexibility needed to get the most out of their machines, while simplifying design and production standards.

View Case Study

Download our CNC Retrofit Brochure

cnc-retrofit-brochure
CablesBnK

Is A CNC Retrofit Right for You?

Equipment used in the heavy construction, power generation and aerospace industries can make good candidates for a retrofit since they typically are older, large machines made with “good iron,” and not easily replaced. Many of these start to fail due to their aging electronics, but due to their large size it is not cost effective to replace the entire machine. In these cases, a CNC retrofit is an excellent option.

Request A Quote

CNC retrofits vs. new machines

A retrofit costs significantly less than a new machine, especially when taking into consideration the hidden costs, such as tooling, fixturing, rigging and foundation. Additionally, new machines may require additional training for the operators and maintenance personnel.

New FANUC CNCs provide better performance

New FANUC CNCs feature high-speed machining functions, which can speed up processing and reduce cycle times by as much as 50 percent. New CNC technologies, such as block look ahead, acceleration and deceleration before and after interpolation, nano-interpolation, nano-smoothing and automatic feedrate control, can be applied to make machine tools more stable and accurate.

FANUC CNC retrofits benefit 5-axis machines

In the past, limited CNC technology made 5-axis machining inefficient, so that any changes in machine, workpiece, workpiece fixtures or tooling required revisiting the CAM system. With features such as tool center point control and 3D workpiece error correction, 5-axis workflow can now be as efficient as 3-axis with any changes adjusted right on the CNC.

CNC retrofits can cut costs

Continuing to run legacy equipment has a number of hidden costs, such as the time taken to source older replacement controls. This can lead to significantly longer total downtime and production losses.

cnc-controls

 

How to Maximize A FANUC CNC Retrofit

To get the most out of a CNC retrofit, upgrading the servo and spindle system to a high-speed, digital interface is critical. If the servo and spindle system can’t keep up with the CNC block processing rate, the tool path will not be accurate. . If an older machine tool is communicating through an analog interface to the servo and spindle system, this will impact the speed and accuracy of the system. Modern FANUC CNCs are highly integrated and communicate over high-speed fiber optic cables to the servo and spindle system, which create the high-performance systems needed to deliver the smoothest surface finish on contoured surfaces.

Retrofits can save energy

When servo and spindle motors of a machine tool continuously accelerate and decelerate as they change speed and direction during machining, they use energy and, respectively, give off energy as heat. However, new digital drives incorporate advanced electronics that regenerate electrical energy back to the factory when decelerating the servo and spindle motors. When combined with the low loss power devices and machining processes provided by the CNC, machine electricity costs can be reduced by as much as 50 percent.

Is a CNC retrofit and CNC conversion the same?

To perform a CNC retrofit, equipment must already have a CNC. A CNC conversion involves converting a manual machine into a CNC machine.

Talk to our retrofit experts today!

From old to new again; FANUC breathes new life into old machines.

Augusta Machine before retrofitting

Before Retrofit

Augusta Machine after retrofitting

After Retrofit

Blanchard machine before retrofitting

Before Retrofit

Blanchard machine after retrofitting

After Retrofit

Fellows machine before retrofitting

Before Retrofit

Fellows machine after retrofitting

After Retrofit

Fellows machine before retrofitting

Before Retrofit

Fellows machine after retrofitting

After Retrofit

Bourn & Koch machine before retrofitting

Before Retrofit

Bourn & Koch machine after retrofitting

After Retrofit

Toshiba machine before retrofitting

Before Retrofit

Toshiba machine after retrofitting

After Retrofit